256MB x16 bit IFC nor flash interface with T2080

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

256MB x16 bit IFC nor flash interface with T2080

1,481 Views
rajeshsubramani
Contributor I

Hi,

I am using T2080 in my application in this I planned to connect S70GL02GS12FHIV20 nor flash to the IFC bus. I planned to use x16 bit external latch for address/date demux application. How to interface this devices, My flash is having 27bit addressing.

Regards,

Rajesh

0 Kudos
Reply
4 Replies

1,102 Views
LPP
NXP Employee
NXP Employee

Connections should be as shown in RM Figures 13-277, 13-326

ADM MODE 0, CSOR0[ADM_SHFT]=4

[IFC_AD[0:15],IFC_AVD] -> latch -> A[26:11]

IFC_A[20:30]    ->    A[10:0]

IFC_AD[0:15]    <->    DQ[15:0]

IFC_CS0#    ->    CE#

IFC_OE#        ->    OE#

IFC_WE0#    ->    WE#

IFC_WP0#    ->    WP#

IFC_RB0#    ->    R/B#

1.8V        ->    VIO

3.3V        ->    VCC

PORESET#    ->    RESET#

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,102 Views
fdm
Contributor IV

Hi Pavel,

Should it be "IFC_A[16:26]    ->    A[10:0]"  instead of  "IFC_A[20:30]    ->    A[10:0]"  ?

BR,

Denis

0 Kudos
Reply

1,102 Views
rajeshsubramani
Contributor I

Hi,

Thanks for the recommendation, As per your recommendation I need to provide latch for 16bits(AD0 to AD15) instead I have connected like this whether this will work ?

IFC_A[16:30]    ->    A[14:0]

[IFC_AD[4:15] -> latch -> A[26:15]

IFC_AD[0:15]    <->    DQ[15:0]

IFC_CS0#    ->    CE#

IFC_OE#        ->    OE#

IFC_WE0#    ->    WE#

IFC_WP0#    ->    WP#

IFC_RB0#    ->    R/B#

1.8V        ->    VIO

3.3V        ->    VCC

Regards,

Rajesh

0 Kudos
Reply

1,102 Views
LPP
NXP Employee
NXP Employee

Yes. It will work.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply