bsc9132 Network card driver problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bsc9132 Network card driver problem

2,516件の閲覧回数
zhengguangzhe
Contributor I

For the problem of network card driver of bsc9132, the last engineer only modified DTB adjustment to be used, but has not found the reason why the modification of DTB can be used. Could someone please tell me the principle

0 件の賞賛
返信
1 返信

2,379件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Wang xiaobin,

In Linux Kernel, in arch/powerpc/boot/dts/fsl/bsc9132qds.dtsi, please modify the MDIO PHY address(reg property) according to your target board. Please configure the PHY driver in Kernel configuration file.

        mdio@24000 {
                phy0: ethernet-phy@0 {
                        reg = <0x0>;
                };

 

                phy1: ethernet-phy@1 {
                        reg = <0x1>;
                };

 

                tbi0: tbi-phy@11 {
                        reg = <0x1f>;
                        device_type = "tbi-phy";
                };
        };

 

        enet0: ethernet@b0000 {
                phy-handle = <&phy0>;
                tbi-handle = <&tbi0>;
                phy-connection-type = "sgmii";
        };

 

        enet1: ethernet@b1000 {
                phy-handle = <&phy1>;
                tbi-handle = <&tbi0>;
                phy-connection-type = "sgmii";
        };

 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信