bsc9132 Network card driver problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bsc9132 Network card driver problem

2,508 次查看
zhengguangzhe
Contributor I

For the problem of network card driver of bsc9132, the last engineer only modified DTB adjustment to be used, but has not found the reason why the modification of DTB can be used. Could someone please tell me the principle

0 项奖励
回复
1 回复

2,371 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Wang xiaobin,

In Linux Kernel, in arch/powerpc/boot/dts/fsl/bsc9132qds.dtsi, please modify the MDIO PHY address(reg property) according to your target board. Please configure the PHY driver in Kernel configuration file.

        mdio@24000 {
                phy0: ethernet-phy@0 {
                        reg = <0x0>;
                };

 

                phy1: ethernet-phy@1 {
                        reg = <0x1>;
                };

 

                tbi0: tbi-phy@11 {
                        reg = <0x1f>;
                        device_type = "tbi-phy";
                };
        };

 

        enet0: ethernet@b0000 {
                phy-handle = <&phy0>;
                tbi-handle = <&tbi0>;
                phy-connection-type = "sgmii";
        };

 

        enet1: ethernet@b1000 {
                phy-handle = <&phy1>;
                tbi-handle = <&tbi0>;
                phy-connection-type = "sgmii";
        };

 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复