IPC Compilation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPC Compilation

2,753件の閲覧回数
oscarcarrascoqu
Contributor I

I'm using BSC9131RDB. I am trying to compile IPC provided in BSP Release version (WUSDK_1.0) but some errors have appeared during the compilation process. For details, please refer to the following code:

for dir in fsl_shm dsp_boot ipc; do \

make -C $dir;\

done

make[1]: Entering directory `/home/lte/Desktop/ipc/fsl_shm'

/opt/eldk-5.2.1/powerpc-e500v2/sysroots/i686-eldk-linux/usr/bin/ppce500v2-linux-gnuspe/powerpc-e500v2-gcc -c ./lib/lg_shm.c -I ./lib -I ./include -Wall -o ./lib/lg_shm.o

ar rcs liblg_shm.a ./lib/lg_shm.o

/opt/eldk-5.2.1/powerpc-e500v2/sysroots/i686-eldk-linux/usr/bin/ppce500v2-linux-gnuspe/powerpc-e500v2-gcc ./test/app.c -I ./lib -I ./include -Wall -L. -llg_shm -o app

make[1]: Leaving directory `/home/lte/Desktop/ipc/fsl_shm'

make[1]: Entering directory `/home/lte/Desktop/ipc/dsp_boot'

/opt/eldk-5.2.1/powerpc-e500v2/sysroots/i686-eldk-linux/usr/bin/ppce500v2-linux-gnuspe/powerpc-e500v2-gcc -I /drivers/misc -I ../fsl_shm/include -Wall ./dsp_boot.c ../fsl_shm/lib/lg_shm.c  -o dsp_bt

./dsp_boot.c:37:25: fatal error: fsl_het_mgr.h: No such file or directory

compilation terminated.

make[1]: *** [dsp_bt] Error 1

make[1]: Leaving directory `/home/lte/Desktop/ipc/dsp_boot'

make[1]: Entering directory `/home/lte/Desktop/ipc/ipc'

/opt/eldk-5.2.1/powerpc-e500v2/sysroots/i686-eldk-linux/usr/bin/ppce500v2-linux-gnuspe/powerpc-e500v2-gcc -c ./lib/fsl_usmmgr.c -lpthread -I ./include -I../fsl_shm/include -I /drivers/misc -Wall -o ./lib/fsl_usmmgr.o

./lib/fsl_usmmgr.c:17:23: fatal error: fsl_types.h: No such file or directory

compilation terminated.

make[1]: *** [mem_lib] Error 1

make[1]: Leaving directory `/home/lte/Desktop/ipc/ipc'

make: *** [all] Error 2

I think some files are not included in the BSP that Freescale provided me.

Could someone send me the files that are not included in the package? 

ラベル(1)
0 件の賞賛
返信
0 返答(返信)