How to run SmartDSP OS demos?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run SmartDSP OS demos?

1,321件の閲覧回数
alexanderpolovn
Contributor I

I am trying to run demos for SmartDSP OS on BSC9131RDB.

When I  boot dsp image using command

/ipc/dsp_bt aic_loopback_9x31_rel.bin

I get following response

root@bsc913x:~# /ipc/dsp_bt /media/sda1/dsp/aic_loopback_9x31_rel.bin

===DSP boot Application===(1.1.02)==

SYSTEM MAP

DSP PrivArea: Addr=38000000 Size=8000000

Shared CtrlArea: Addr=37000000 Size=1000000

DSP Core0 M2: Addr=b0000000 Size=80000

DSP Core1 M2: Addr=0 Size=0

DSP M3: Addr=0 Size=0

PA CCSRBAR: Addr =ff700000 Size=100000

DSP CCSRBAR: Addr =ff600000 Size=100000

PA Shared Area: Addr=10000000 Size=f000000

DSP Shared Area: Addr=1f000000 Size=1000000

DSP READY SET

Copy Part b0000000 124b6

Copy Part b0014000 2f0c

Copy Part ff618108 4

DSP image copied

sleep 4 sec

DSP HW Sem1 value not correctly set, value=0

DSP Boot Failed, Please reset

The same result I get for other demos.

I will appriciate any help.

Alexander Polovnikov

ラベル(1)
0 件の賞賛
返信
1 返信

1,158件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Please ignore the message.

0 件の賞賛
返信