How to run SmartDSP OS demos?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to run SmartDSP OS demos?

1,320 次查看
alexanderpolovn
Contributor I

I am trying to run demos for SmartDSP OS on BSC9131RDB.

When I  boot dsp image using command

/ipc/dsp_bt aic_loopback_9x31_rel.bin

I get following response

root@bsc913x:~# /ipc/dsp_bt /media/sda1/dsp/aic_loopback_9x31_rel.bin

===DSP boot Application===(1.1.02)==

SYSTEM MAP

DSP PrivArea: Addr=38000000 Size=8000000

Shared CtrlArea: Addr=37000000 Size=1000000

DSP Core0 M2: Addr=b0000000 Size=80000

DSP Core1 M2: Addr=0 Size=0

DSP M3: Addr=0 Size=0

PA CCSRBAR: Addr =ff700000 Size=100000

DSP CCSRBAR: Addr =ff600000 Size=100000

PA Shared Area: Addr=10000000 Size=f000000

DSP Shared Area: Addr=1f000000 Size=1000000

DSP READY SET

Copy Part b0000000 124b6

Copy Part b0014000 2f0c

Copy Part ff618108 4

DSP image copied

sleep 4 sec

DSP HW Sem1 value not correctly set, value=0

DSP Boot Failed, Please reset

The same result I get for other demos.

I will appriciate any help.

Alexander Polovnikov

标签 (1)
0 项奖励
回复
1 回复

1,157 次查看
lunminliang
NXP Employee
NXP Employee

Please ignore the message.

0 项奖励
回复