Firmware Image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware Image

4,064 Views
latha_g
Contributor II

Hi Team,

We are using custom ls2088ardb board and we are using lsdk 18.09 sdk.

We are able to build a firmware image for qspi board.

flex-builder -i mkfw -m ls2088ardb -b qspi

We are able to get the logs but the kernel fails to boot as Image is unable to boot we need to make changes such that it takes uimage.bin file.

I have made changes in manifest file but still i get this error.

Wrong Image Format for bootm command
ERROR: can't get kernel image!

can you please guide me further

0 Kudos
Reply
1 Reply

3,922 Views
Pavel
NXP Employee
NXP Employee

Is there error message from u-boot o your board?

Is your "bootm" command similar to "bootm" command from the Section 4.6.6.3 of LSDK 1809 User Guide?

Have a great day,
Pavel Chubakov

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply