Processor Expert软件知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor Expert Software Knowledge Base

讨论

排序依据:
See how a full MQX Lite application works, how the tasks are implemented, and how they interact with other components.
查看全文
Product Information on Freescale.com Product Summary Page Documentation Downloads Training and support
查看全文
The attached document shows how tou use Processor Expert Driver Suit to generate code for IAR. You can see details in the notes at the botton of the slides. Best regards, Carlos
查看全文
GDisplay Description Component which implements drawing routines (line, rectangle, circle, ...) for a graphical display Component GDisplay.PEupd Dependencies Display, FreeRTOS License License : Open Source (LGPL) Copyright : (c) Copyright Erich Styger, 2011, all rights reserved. This an open source software in the form of a Processor Expert Embedded Component. This is a free software and is opened for education, research and commercial developments under license policy of following terms: * This is a free software and there is NO WARRANTY. * No restriction on use. You can use, modify and redistribute it for personal, non-profit or commercial product UNDER YOUR RESPONSIBILITY. * Redistributions of source code must retain the above copyright notice.
查看全文
GenericTimeDate Description Generic Time/Date handling. Component GenericTimeDate.PEupd Dependencies none License (c) Copyright Freescale Semiconductor, 2012 http: www.freescale.com Source code is based on the original TimeDate Processor Expert component.
查看全文
SSEC Description Security Driver for the SPHY component Component SSEC.PEupd Dependencies Wait License License : Open Source (LGPL) Copyright : (c) Copyright Erich Styger, 2012, all rights reserved. This an open source software implementing a driver using Processor Expert. This is a free software and is opened for education, research and commercial developments under license policy of following terms: * This is a free software and there is NO WARRANTY. * No restriction on use. You can use, modify and redistribute it for personal, non-profit or commercial product UNDER YOUR RESPONSIBILITY. * Redistributions of source code must retain the above copyright notice.
查看全文
FreeRTOS Description FreeRTOS (www.freertos.org) implementation as component. Support for all S08 and all S12(X), ColdFire V1 (CN, JM, QE, JE, and MM families), ColdFire V2 (5225x) and all Kinetis (tested with K40, K60, K70/M4F, KL20Z Freedom Board). Component FreeRTOS.PEupd Dependencies Utility, FreeRTOSTrace, PercepioTrace A tutorial how to use the FreeRTOS Embedded Processor Expert component is used can be found here: Tutorial: FreeRTOS on DEMOJM Attention Classic (non-eclipse) Users! The component has been tested with CodeWarrior for S12(X) V5.1, which is not eclipse based. The eclipse based CodeWarrior (MCU10.x) is using the concept of an RTOS adapter. The FreeRTOS component has now a setting to disable this. You need to set the setting 'Classic CodeWarrior' to 'yes' in order to have it working in a non-eclipse CodeWarrior environment. Otherwise you will see internal errors during code generation. Additionally at least the PE 3.09 Service pack needs to be installed. The update is available on http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_UPDATES_MCU_63, direct link:CodeWarrior for MCU V6.3 Processor Expert V3.09 Update License License : Open Source (LGPL) FreeRTOS (c) Copyright 2003-2012 Richard Barry, http: www.FreeRTOS.org FreeRTOS Processor Expert Component: (c) Copyright Erich Styger, 2012 Processor Expert and CodeWarrior (c) Copyright Freescale Semiconductor, 2012, all rights reserved This is a free software and is opened for education, research and commercial developments under license policy of following terms: * This is a free software and there is NO WARRANTY. * No restriction on use. You can use, modify and redistribute it for personal, non-profit or commercial product UNDER YOUR RESPONSIBILITY. * Redistributions of source code must retain the above copyright notice.
查看全文
Product Information on Freescale.com Product Summary Page Documentation Downloads Buy/Specifications
查看全文
Training Videos Processor Expert - Introduction (CodeWarrior) (Video - 03:53) - Learn the Processor Expert UI, what components are, and how to add one to a project in the CodeWarrior Development Studio. Processor Expert - Working with Components (CodeWarrior) (Video - 04:00) - Learn how to add, configure, and remove a component, and how to generate code in CodeWarrior Development Studio. Processor Expert - The Code Model (CodeWarrior) (Video - 04:41) - Using CodeWarrior Development Studio, learn the answers to the questions, What code does Processor Expert generate? Where does it put the code? And how do I use it? Creating an MQX Lite Project (CodeWarrior) (Video - 05:58) - Using CodeWarrior Development Studio, learn how to create an MQX Lite component from scratch. You'll also learn where Processor Expert puts the task functions and the RTOS code itself. An MQX Lite Example (CodeWarrior) (Video - 05:15) - See how a full MQX Lite application works, how the tasks are implemented, and how they interact with other components. Exporting and Importing Templates (CodeWarrior) (Video - 04:02) - Learn how to export and import a file that can completely configure and generate the code required for an arbitrarily complex hardware and software system.
查看全文