shared adc component

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

shared adc component

跳至解决方案
2,300 次查看
bataliero
Contributor III

Hi ,

Is it possible to create shared ADC component on Kinetis K60 ? I have to get values from 4 pins on ADC0 and ADC1 . It would be more elegant to do not have duplicated code like

LDD_TError Adc0_GetMeasuredValues(LDD_TDeviceData *DeviceDataPtr, LDD_TData *BufferPtr)

{

  uint8_t Sample;

  AdConv0_TResultData *pBuffer = (AdConv0_TResultData *)BufferPtr;

  /* Copy values from result registers defined in the active sample

     group to the user supplied buffer */

  for (Sample = 0U; Sample < ((AdConv0_TDeviceDataPtr)DeviceDataPtr)->SampleCount; Sample++) {

    pBuffer[Sample] = (uint16_t)(ADC_PDD_GetResultValueRaw(ADC0_BASE_PTR, Sample));

  }

  return ERR_OK;                       /* OK */

}

LDD_TError Adc1_GetMeasuredValues(LDD_TDeviceData *DeviceDataPtr, LDD_TData *BufferPtr)

{

  uint8_t Sample;

  AdConv1_TResultData *pBuffer = (AdConv1_TResultData *)BufferPtr;

  /* Copy values from result registers defined in the active sample

     group to the user supplied buffer */

  Sample = ((AdConv1_TDeviceDataPtr)DeviceDataPtr)->SampleCount;

  for (Sample = 0U; Sample < ((AdConv1_TDeviceDataPtr)DeviceDataPtr)->SampleCount; Sample++) {

    pBuffer[Sample] = (uint16_t)(ADC_PDD_GetResultValueRaw(ADC1_BASE_PTR, Sample));

  }

  return ERR_OK;                       /* OK */

}

0 项奖励
回复
1 解答
1,951 次查看
ProcessorExpert
Senior Contributor III

Hello,

as far as I know that this is not currently supported in ADC. Anyway I have passed this as feature request to developers.

best regards

Vojtech Filip

Processor Expert Support Team


在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,952 次查看
ProcessorExpert
Senior Contributor III

Hello,

as far as I know that this is not currently supported in ADC. Anyway I have passed this as feature request to developers.

best regards

Vojtech Filip

Processor Expert Support Team


0 项奖励
回复
1,951 次查看
elisamejia
Contributor III

Hello!

Is it possible to do it now using the K70 tower module? I have to digitize 3 different signals and show them in a TWR-LCD-RGB. I want to use the tower elevator connections so I have no access to ADC2 or ADC3. When I create my first ADC0 and ADC1 objects in ProcessorExpert, it works fine; however, when I create the other one, using ADC0 or ADC1 in a different pin, it says that AD converter is already used by the other component, and if I enable the sharing option it says that this mode isn't supported on this version of module.

How can I accomplish my 3 simultaneous ADC reads?

Best regards,

Elisa

0 项奖励
回复