sbc_fs651 component is not available in processor expert of mpc5777c controller.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sbc_fs651 component is not available in processor expert of mpc5777c controller.

1,566 Views
Krishnayya29
Contributor I

Hi Nxp,

 

when i import SBC example from NXP for MPC5777c controller, IDE Says that  sbc_fs651 is not installed in this version .Could you please help me out to enable this component to make this example work properly. i am using ide  S32DS power 2.1  and RTM 3.0.3 SDK version.i pasted image that shows  error messages and disabled component below.

Krishnayya29_0-1681910361547.png

Please let me know if i need to communicate with SBC via SPI component, if  sbc_fs651 is not available for this controller or SDK.

Thanks,

Krishnayya

0 Kudos
Reply
4 Replies

1,473 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Have a look at this thread where one customer solved this issue:

https://community.nxp.com/t5/MPC5xxx/I-get-the-following-error-when-i-laund-the-S32-IDE/m-p/1616682#...

Best regards,

Peter

0 Kudos
Reply

1,550 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, I have just opened new project from example and everything looks fine.

petervlna_0-1681976945720.png

Do you have the correct components installed?

petervlna_1-1681977030028.pngpetervlna_2-1681977088097.png

Best regards,

Peter

0 Kudos
Reply

1,547 Views
Krishnayya29
Contributor I

Hi Peter,

Thanks for the quick reply.i am not getting option to select version PA15 or PA11 as you.i need to install PA15  SDK version.can you please guide me to  to install PA15sdk .

the pop up i am getting from IDE is pasted below.

Krishnayya29_0-1681979159523.png

Thanks,

Krishnayya

 

0 Kudos
Reply

1,501 Views
Krishnayya29
Contributor I

Hi Peter,

 

Could you please tell me what i am doing wrong while installing or which version i need to install to work with SBC.presently i am using S32DS power architecture 2.1 version and SDK 3.0.3.

 

Thanks,

Krishnayya

0 Kudos
Reply