pwm using processor expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pwm using processor expert

3,585 Views
MatteoPioTotta
Contributor I

Hi,

I would create a EPWM using processor expert,how can i make?

0 Kudos
Reply
4 Replies

3,034 Views
ProcessorExpert
Senior Contributor III

Hi,

Could you be more specific what do you mean by EPWM? Which CPU do you use?

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply

3,034 Views
MatteoPioTotta
Contributor I

Hi,

EPWM mean EDGE ALIGNED PWM BUT I CAN'T INITIALIZE NEVER THINGS WITH

PROCESSOR EXPERT...I DON'T KNOW BUT DEVICE INITIALIZATION WORK....NOW I

HAVE A NEW PROBLEM WHEN I TRY TO RUN MY PROJECT,AFTER THAT I CORECCTLY

BUILD IT,THAT IS:

"Description:

Launch hook com.freescale.cdt.launch.cw.

TerminateAndRestartHook@14b5f16 failed with internal errors while

checking launch

Explanation:

No details available.Stack Trace:

[Ljava.

lang.StackTraceElement;@1e386bc"

IF YOU CAN RESOLVE THIS PROBLEM I

THANK YOU A LOT.

BEST REGARD

MATTEO TOTTA

-


Messaggio

originale----

Da: [email protected]

Data: 17/09/2012 16.14

A: "Matteo Totta"<[email protected]>

Ogg: Re: [Processor Expert

Software] - pwm using processor expert

Processor Expert [https:

//community.freescale.com/people/ProcessorExpert] created the

discussion

"pwm using processor expert"

To view the discussion,

visit: https://community.freescale.com/message/300953#300953

0 Kudos
Reply

3,034 Views
Petr_H
NXP Employee
NXP Employee

This is strange, we are not aware of such problem.

Please try to reinstall the CodeWarrior and if it doesn't help create a service request using the command Support > Technical Service Request on www.freescale.com.

best regards

Petr Hradsky

Processor Expert Support Team

0 Kudos
Reply

3,034 Views
MatteoPioTotta
Contributor I

Thanks but now i can use Device Initialization,

This tool don't make any problem.

best regards

Matteo Totta

0 Kudos
Reply