pwm using processor expert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pwm using processor expert

3,656件の閲覧回数
MatteoPioTotta
Contributor I

Hi,

I would create a EPWM using processor expert,how can i make?

0 件の賞賛
返信
4 返答(返信)

3,105件の閲覧回数
ProcessorExpert
Senior Contributor III

Hi,

Could you be more specific what do you mean by EPWM? Which CPU do you use?

best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信

3,105件の閲覧回数
MatteoPioTotta
Contributor I

Hi,

EPWM mean EDGE ALIGNED PWM BUT I CAN'T INITIALIZE NEVER THINGS WITH

PROCESSOR EXPERT...I DON'T KNOW BUT DEVICE INITIALIZATION WORK....NOW I

HAVE A NEW PROBLEM WHEN I TRY TO RUN MY PROJECT,AFTER THAT I CORECCTLY

BUILD IT,THAT IS:

"Description:

Launch hook com.freescale.cdt.launch.cw.

TerminateAndRestartHook@14b5f16 failed with internal errors while

checking launch

Explanation:

No details available.Stack Trace:

[Ljava.

lang.StackTraceElement;@1e386bc"

IF YOU CAN RESOLVE THIS PROBLEM I

THANK YOU A LOT.

BEST REGARD

MATTEO TOTTA

-


Messaggio

originale----

Da: [email protected]

Data: 17/09/2012 16.14

A: "Matteo Totta"<[email protected]>

Ogg: Re: [Processor Expert

Software] - pwm using processor expert

Processor Expert [https:

//community.freescale.com/people/ProcessorExpert] created the

discussion

"pwm using processor expert"

To view the discussion,

visit: https://community.freescale.com/message/300953#300953

0 件の賞賛
返信

3,105件の閲覧回数
Petr_H
NXP Employee
NXP Employee

This is strange, we are not aware of such problem.

Please try to reinstall the CodeWarrior and if it doesn't help create a service request using the command Support > Technical Service Request on www.freescale.com.

best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信

3,105件の閲覧回数
MatteoPioTotta
Contributor I

Thanks but now i can use Device Initialization,

This tool don't make any problem.

best regards

Matteo Totta

0 件の賞賛
返信