package view not showing core elements from target MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

package view not showing core elements from target MCU

ソリューションへジャンプ
1,864件の閲覧回数
GMVS
Contributor III

Hi

i've got access to two computers with Code Warrior 10.2

in one of them (windows 7) the package view shows the MCU complete, with the core blocks and the pin names
but in the other (windows xp), it only says the name of the MCU without showing  core blocks, pin names, grounds, etc; it just shows the blanck green square there with the right name

does anyone knows how can i enable those features? because it doesnt shows them despite i change from MCU

 

thanks

0 件の賞賛
返信
1 解決策
1,761件の閲覧回数
ProcessorExpert
Senior Contributor III

Hi,

the details are not visible in case the window is too small. Have you tried to use the magnifier glass icon :smileyplus: ?

 

best regards
Petr Hradsky
Processor Expert Support Team

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,762件の閲覧回数
ProcessorExpert
Senior Contributor III

Hi,

the details are not visible in case the window is too small. Have you tried to use the magnifier glass icon :smileyplus: ?

 

best regards
Petr Hradsky
Processor Expert Support Team

 

0 件の賞賛
返信