package view not showing core elements from target MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

package view not showing core elements from target MCU

Jump to solution
1,868 Views
GMVS
Contributor III

Hi

i've got access to two computers with Code Warrior 10.2

in one of them (windows 7) the package view shows the MCU complete, with the core blocks and the pin names
but in the other (windows xp), it only says the name of the MCU without showing  core blocks, pin names, grounds, etc; it just shows the blanck green square there with the right name

does anyone knows how can i enable those features? because it doesnt shows them despite i change from MCU

 

thanks

0 Kudos
Reply
1 Solution
1,765 Views
ProcessorExpert
Senior Contributor III

Hi,

the details are not visible in case the window is too small. Have you tried to use the magnifier glass icon :smileyplus: ?

 

best regards
Petr Hradsky
Processor Expert Support Team

 

View solution in original post

0 Kudos
Reply
1 Reply
1,766 Views
ProcessorExpert
Senior Contributor III

Hi,

the details are not visible in case the window is too small. Have you tried to use the magnifier glass icon :smileyplus: ?

 

best regards
Petr Hradsky
Processor Expert Support Team

 

0 Kudos
Reply