mingw32-make error problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mingw32-make error problem

1,604 次查看
Embionics
Contributor III

Hello,

I am working with KL25Z128VLH4 on CW10.3.

I am using UART1 and UART0 in this controller.

I am defining a structure for UART in my HWApi.h file.

typedef struct

{

  LDD_TDeviceData* DeviceDataPrv1;

  volatile uint8_t isSent; /* this will be set to 1 once the block has been sent */

  uint8_t rxChar; /* single character buffer for receiving chars */

  uint8_t (*rxPutFct)(uint8_t); /* callback to put received character into buffer */

} UART_Desc;

UART_Desc deviceData_UART0,deviceData_UART1;

I am using "deviceData_UART0" for UART0 and "deviceData_UART1" for UART1.

Now in Event.c file I have to use this structure.

But when I included HWApi.h file in Event.c file an error occurred as

mingw32-make: *** [VTS_Code_64Pin.elf] Error 1


I am not getting what is the meaning of this type of error?

But when I copied(redefined ) above structure in Event.c as it is,without including HWApi.h file it works.

Both files are located in local "sources" folder.

-Amreen

标记 (3)
0 项奖励
回复
1 回复

1,329 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Amreen:

Are you including the necessary header files inside of HWApi.h? The structure you want to define includes no-standard types.

e.g. LDD_TDeviceData type is declared in PE_Types.h (I assume you use Processor Expert).

When you declare it in Events.c, this file includes Events.h, which respectively calls PE_Types.h.

Hope this helps!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------