_lwevent_create() causes Unhandled_ivINT_Hard_Fault interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

_lwevent_create() causes Unhandled_ivINT_Hard_Fault interrupt

1,485 Views
zacharywalton
Contributor I

I am using MQX_Lite on a FRDM-KE06Z dev board, and when I try to create a lwevent group at the beginning of a task, the Unhandled_ivINT_Hard_Fault ISR is called.  I have lwevents enabled in the MQX_Lite PEx Component, but is there something else that I need to include to be able to use them?

0 Kudos
Reply
1 Reply

1,216 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Zachary Walton:

Could you tell me what software (CodeWarrior, KDS, PE Driver Suite) and the version you are using?

For example I tried to create a MQX Lite project in CodeWarrior v10.6 for the KE06 and I did not see a hardfault when creating a LWEVENT. That is why I need more information to replicate the issue and report it to developers.

Thank you!

Regards,

Jorge Gonzalez

0 Kudos
Reply