imx8mq low power mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq low power mode

2,667件の閲覧回数
Aakash_Sharma
Contributor II

Hi,

We are working imx8mq custom board and require to put processor in low power mode in order to reduce power consumption. As per AN13400 there are two low power modes, 1) Wait and Stop Mode 2) DSM. We have tried DSM mode and it reduces power consumption but also want to try Wait and Stop Mode. So, how to put processor into this mode? 

NOTE: - There are some registers which needs to be configured as per AN13400 but how we can configure them?

AN13400.pdf (nxp.com)

ラベル(2)
0 件の賞賛
返信
1 返信

2,416件の閲覧回数
RachelGomez123
Contributor I

3.2 Low-power modes on i.MX 8M This section describes the specifics of low-power modes on i.MX 8M and the difference between Suspend mode and DSM (Deep Sleep mode). 3.2.1 SoC low-power modes introduction There are two platform low-power modes, Wait and Stop, and one system low-power mode, DSM.

 

Greeting,

Rachel Gomez

0 件の賞賛
返信