imx8mp random reboot issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp random reboot issue

4,797件の閲覧回数
vprajapati
Contributor II

I am working on project in which we are using custom  board having imx8mp processor with 2GB RAM and 16 GB eMMC. I have interfaced 2 MIPI CSI camera (RGB and IR), 5" LCD touch screen, ethernet, IR LEDs, White LED, RGB LEDs, DMIC, Speaker, etc.  

The board gets randomly rebooted while power on. The issue is random. Sometimes it gets booted successfully and sometimes it reboot continuously. 

I am not able to figure out the issue why its get randomly rebooted. However, I have observed several points.

  1. When I remove 2nd (IR) camera, board doesn't reboot.
  2.  When I remove 5" LCD,  but both camera connected the board doesn't reboot.
  3. When I remove IR LEDs (as these are on other small board) the board doesn't reboot.

We have checked the current consumption and its not crossing 500mA with all peripherals. We are using 1A DC Adapter to power up the board.

Attaching logs for your reference. 

0 件の賞賛
返信
5 返答(返信)

4,782件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @vprajapati!

Thank you for contacting NXP Support!

 

Do you perform the correct DDR training?

Try to use a better Power Supply I suggest at least 3A (Like our EVK boards).

 

Best Regards!

Chavira

0 件の賞賛
返信

4,764件の閲覧回数
vprajapati
Contributor II

Hi @Chavira 

Yes,  DDR training is performed and using correct ddr4_timing.c file.

I also used the DC Programmable Power supply with 2A, however the issue still persist. The current consumption is not even crossing that 500mA.  

0 件の賞賛
返信

4,750件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @vprajapati!

Can you share the shcematic?

The peripherals are connected directly to PMIC?

 

If is not possible to upload the schematic you can open a private support ticket in our webpage.

 

 

 

0 件の賞賛
返信

4,710件の閲覧回数
vprajapati
Contributor II

Hi @Chavira,

The PMIC supply is only used for some pullups and other peripherals. Camera and LCD is not getting direct supply from PMIC. It is also used to control some LDOs.


0 件の賞賛
返信

4,698件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @vprajapati!

The principal problem should be your power delivery from the peripherals that are you using.

 

I recommend to check every power rail of your board and do double check to your design.

 

You can consult the i.MX 8M Plus Hardware Developer’s Guide.

 

 

 

0 件の賞賛
返信