eth0 tx fail for bsc9132

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eth0 tx fail for bsc9132

1,124件の閲覧回数
zhengguangzhe
Contributor I

hello

    Recently, we encountered an abnormal problem with the ethernet eth0.

it can't send packets but can receive packets. We analyzed and found:

1、The interrupt eth0_g_tx has no changed;

2、Transmit status register (eTSECx_TSTAT) always is 00 00 ff 00
3、kernel code sch_generic.c-->dev_watchdog Masked timeout processing logic

if (some_queue_timedout) {
                char drivername[64];
                WARN_ONCE(1, KERN_INFO "NETDEV WATCHDOG: %s (%s): transmit queue %u timed out\n",
                       dev->name, netdev_drivername(dev, drivername, 64), i);
                /* dev->netdev_ops->ndo_tx_timeout(dev); */
            }

My questions:

1、Under what conditions will this problem occur?

2、Is the timeout processing to solve this problem?

3、Is the chip itself defective?

 

0 件の賞賛
返信
0 返答(返信)