error in component bean eeprom in 9s12g128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error in component bean eeprom in 9s12g128

2,407件の閲覧回数
ThinkChip_Vendi
Contributor I

Hi, I have a error when I add the component eeprom, the error says 

+IEE1
+ERROR: Compiler option -CpPPAGE=0x15 (address of PPAGE register) or -CpPPAGE=RUNTIME must be set to compile the generated code correctly (current target settings, Compiler for HC12, Options, Code Generation tab, PPAGE register is used for paging). After compiler option change, run Code design to apply the change in Processor Expert. For details, see Help of the component.

+IEE1
+ERROR: There are errors in component, it is impossible to generate code

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,987件の閲覧回数
ThinkChip_Vendi
Contributor I

I do all steps, and still have the same error, thanks

0 件の賞賛
返信

1,987件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

could you please provide the verison of PE and CW that you use?

 

best regards
Vojtech Filip
Processor Expert Support Team

0 件の賞賛
返信