error in component bean eeprom in 9s12g128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error in component bean eeprom in 9s12g128

1,673 次查看
ThinkChip_Vendi
Contributor I

Hi, I have a error when I add the component eeprom, the error says 

+IEE1
+ERROR: Compiler option -CpPPAGE=0x15 (address of PPAGE register) or -CpPPAGE=RUNTIME must be set to compile the generated code correctly (current target settings, Compiler for HC12, Options, Code Generation tab, PPAGE register is used for paging). After compiler option change, run Code design to apply the change in Processor Expert. For details, see Help of the component.

+IEE1
+ERROR: There are errors in component, it is impossible to generate code

 

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,254 次查看
ThinkChip_Vendi
Contributor I

I do all steps, and still have the same error, thanks

0 项奖励
回复

1,254 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

could you please provide the verison of PE and CW that you use?

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复