bug in MKL04Z16VFK4 CPU component?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bug in MKL04Z16VFK4 CPU component?

ソリューションへジャンプ
1,431件の閲覧回数
bowerymarc
Contributor V

It looks like the memory size and range is incorrect in then CPU component for MKL04Z16VFK4.  The '8 and '32 seem OK.

KL04Z16VFK4 bug.png

With this setting, programs loading get a Hard Fault within __copy_rom_sections_to_ram()

Changing address to 1FFFFE00 and size to 800 (which matches the screwy data sheet formula, and the actual amount of SRAM on the chip) and the fault goes away.

M

ラベル(1)
0 件の賞賛
返信
1 解決策
1,338件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I confirm that it's a bug in Processor Expert. We will fix it for the next Processor Expert release. You have correctly identified the workaround.

We are sorry for the inconvenience.

Best regards

Petr Hradsky

Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,339件の閲覧回数
Petr_H
NXP Employee
NXP Employee

Hi,

I confirm that it's a bug in Processor Expert. We will fix it for the next Processor Expert release. You have correctly identified the workaround.

We are sorry for the inconvenience.

Best regards

Petr Hradsky

Processor Expert Support Team

0 件の賞賛
返信