Wrong Touch Detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wrong Touch Detection

1,974 Views
taimurwajad123
Contributor III

Hello All,

We are using TSS 3.1 library and TSI module. Recently we found a problem in our HMI, when interference(EMI) is injected upon HMI electrodes there comes a situaion when one or more electrodes are being permanently detected as pressed untill new startup.

After detailed analysis we found out that when inetreference is injected then there comes a situation when Baseline signal adopts itself to a lesser value than Instant signal and its always detecting as touch because Instant delta remains higher than our electrode threshold and baseline will not adopt itself untill release has been detetcted.

Anyone else faced the same issue? or any leads how we can fix it?

We are using Kinetis K10 uc with Processor expert having 8 electrodes. 

0 Kudos
Reply
1 Reply

1,841 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Are you setting the autocalibration function? also, there is a manual calibration or hardware recalibration ( I do not remember which one reset the baseline), I recommend you do the calibration after some time.

Also, you can change the N samples to get better results

regards

Vicente Gomez

0 Kudos
Reply