When i was running my programme in a for loop, it can loop 3 time and in fourth times, it shows Unhandled int code, what should i do ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When i was running my programme in a for loop, it can loop 3 time and in fourth times, it shows Unhandled int code, what should i do ?

2,552 次查看
lammanhuen926
Contributor I

Here is my code, the colours are just making LED flash in different colour and FAIL is pink light

/* ###################################################################
**     Filename    : main.c
**     Project     : Assginment 1
**     Processor   : MKL25Z128VLK4
**     Version     : Driver 01.01
**     Compiler    : GNU C Compiler
**     Date/Time   : 2018-11-08, 10:09, # CodeGen: 0
**     Abstract    :
**         Main module.
**         This module contains user's application code.
**     Settings    :
**     Contents    :
**         No public methods
**
** ###################################################################*/
/*!
** @file main.c
** @version 01.01
** @brief
**         Main module.
**         This module contains user's application code.
*/        
/*!
**  @addtogroup main_module main module documentation
**  @{
*/        
/* MODULE main */

/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "Events.h"
#include "RED_LED.h"
#include "TU1.h"
#include "GREEN_LED.h"
#include "BLUE_LED.h"
#include "TU2.h"
#include "TSS1.h"
#include "AD1.h"
#include "AdcLdd1.h"
#include "stdlib.h"
/* Including shared modules, which are used for whole project */
#include "PE_Types.h"
#include "PE_Error.h"
#include "PE_Const.h"
#include "IO_Map.h"
/* User includes (#include below this line is not maintained by Processor Expert) */
int ispressed=0;
static uint16_t Random;
/*lint -save  -e970 Disable MISRA rule (6.3) checking. */

int main(void)
/*lint -restore Enable MISRA rule (6.3) checking. */
{
  /* Write your local variable definition here */
unsigned char i=0,k,y,p,l,j;
unsigned char Arraycolour[30],Gamecolour[30],Inputcolour[30];
  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  PE_low_level_init();
  /*** End of Processor Expert internal initialization.                    ***/
  /* Write your code here */
for (;;){                  /*For loop just for looping the game */
 ALLOFF();
 k=0,y=0,p=5,l=0,j=0;
 ispressed=0;
   AD1_Measure(TRUE);               /* do measurment and wait for the result */
   AD1_GetValue16(&Random);              /* get the result into Random variable */
 srand(Random);
 TSS_Task();
 while(ispressed <2){
  TSS_Task();}

 if(TSS1_cKey0.Position >= 0 && TSS1_cKey0.Position<=64){      /*game start when user touch slider*/
    yellow();                 /*signal for game start*/
   }
 for (y=0;y<p+i;y++){              /*For loop to create random light and store
                                        light signal in to Array*/
        k=rand()%9;
        if(k<=2)
        {BLUELED();
        Arraycolour[j]=1;
        Gamecolour[j]=1;
       Inputcolour[j]=1;}
        else if(k>=3 && k<6)
        {REDLED();
        Arraycolour[j]=2;
        Gamecolour[j]=2;
       Inputcolour[j]=2;}
        else if(k>=6)
        {GREENLED();
        Arraycolour[j]=3;
        Gamecolour[j]=3;
       Inputcolour[j]=3;
        }
       j++;}
   /* y=0;
        for (y=0;y=p;y++){
         if(Arraycolour[y]=1)
                  {BLUELED();}
              else if(Arraycolour[y]=2 )
                  {REDLED();}
              else if(Arraycolour[y]=3)
                 {GREENLED();}}*/
  ALLOFF();
                    /* light signal shows repeat colour with a missing one */
    l=rand()%(p+i);                /* y will random value according to number of round
                         (Round 1 is 0-4, round 2 is 0-5), it will decide
                         where to start to get the light out from array*/
    if (l>=p-i){                /* if loop just prevent the random going too large, think
                         of in loop 3, there are 7 colours, if l==5  while we have
                          to pick up random numbers start from Arraycolour[5], it can
                          only pick up two and 7 is nothing in Arraycolour[7], so by
                          comparing l value is not grater than y-i, it will minus i
                          to get the random l in range of array to pick colours out  */
     l=l-i;
    }
    for (y=0;y<1+i;y++){              /* Make colour missing in an array */
     Gamecolour[l]=0;
     l++;}
    l-=y;                  /* Make l back to origion place for use in array later */
    for (y=0;y<5+i;y++){              /* Displaying missing colour */
     if (Gamecolour[y]==0)
  {white();}
     else if(Gamecolour[y]==1)
     {BLUELED();}
     else if(Gamecolour[y]==2 )
     {REDLED();}
     else if(Gamecolour[y]==3)
     {GREENLED();}}
    for (y=0;y<1+i;y++){
     TSS_Task();
 ispressed=0;
 while(ispressed <2){
  TSS_Task();}            /* Get user input */
wait(250);
     if( TSS1_cKey0.Position >= 0 && TSS1_cKey0.Position<18){
      Gamecolour[l]=2;}
  else if( TSS1_cKey0.Position >= 19 && TSS1_cKey0.Position<48){
   Gamecolour[l]=3;}
  else if( TSS1_cKey0.Position >= 48 && TSS1_cKey0.Position<=64){
   Gamecolour[l]=1;}
      l++;}
    for (y=0;y<5+i;y++){              /* If user input is match Gamecolour, An Array will
                                             store it as 1, if not store it as 0*/
     if(Inputcolour[y]==Gamecolour[y]){
  Arraycolour[y]=1;}
     else {Arraycolour[y]=0;}}
     j=0;
  for (y=0;y<5+i;y++){              /* Adding up values in an array, to determinate final
                                          value of j*/
   j+=Arraycolour[y];}
   if (j==5+i){               /* Check value of j if it match the correct answer */
   i++;
   SKYBLUE();}                /*Light showing all correct and go to next level  */
   else {i=0;
   FAIL();}                /* Light showing wrong input and restart game */
 }
  /* For example: for(;;) { } */
  /*** Don't write any code pass this line, or it will be deleted during code generation. ***/
  /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
  #ifdef PEX_RTOS_START
    PEX_RTOS_START();                  /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of RTOS startup code.  ***/
  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
  for(;;){}
  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/
/* END main */
/*!
** @}
*/
/*
** ###################################################################
**
**     This file was created by Processor Expert 10.5 [05.21]
**     for the Freescale Kinetis series of microcontrollers.
**
** ###################################################################
*/
标记 (1)
0 项奖励
回复
2 回复数

1,229 次查看
jessrobs01
Contributor I

In this code, you are creating a memory game where colors flash in random sequences, and the player must replicate the sequence by touching the corresponding areas on the touchscreen. The colors (blue, red, green) indicate different inputs, and when the player successfully repeats the sequence, they progress to the next level. If the sequence is incorrect, the game shows a "FAIL" light.

If you're looking for a fun, engaging game with similar challenges, play ovo game where you can test your memory and reflexes with various mini-games!

0 项奖励
回复

2,195 次查看
HerbertCunningham
Contributor I
I am also facing the same problem, what is the solution to this problem download mod apkrabi
0 项奖励
回复