Using TPMxCLK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using TPMxCLK

1,389 Views
mahkamehvarza
Contributor I

Could someone please explain to me how I can set up the MC9S08QE32 to use an external clock ref (TPMxCLK) on any of the timer modules, in PE. How do specify which pin is the input clk? How do I specify the xCLK frequency?

I am using Freescale Codewarrior 5.9.0

Thanks for your help in advance.

0 Kudos
Reply
1 Reply

1,311 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

I use CW10.6 , i can configure the external clock source of TPM as this :

pastedImage_0.png

And please  screenshot your CW, and does it have the same view ?

BR

Alice

0 Kudos
Reply