Use procesor expert default problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use procesor expert default problem

跳至解决方案
3,338 次查看
marceladueñas
Contributor II

Hello everybody, i try to update to kds 3.2 and sdk 2.0 , a terrible idea because now all my projects have the next issue: 
ERROR: at line 1: {{DEVELOPMENT}} The symbol "UseProcessorExpertDefault" was used without testing %ifdef or %if defined(). It's recommended to use %get() instead (if possible). (file: Beans\CriticalSection\CriticalSection.chg) V3 CS1 Processor Expert Problem

i try to comeback again , i uninstall all and comeback to the 3.0 version but the issue is the same , an even if i choose freRtos or procesor expert there is an error . I don't know what more can i do. HELP!!!

标签 (1)
1 解答
3,122 次查看
BlackNight
NXP Employee
NXP Employee

Hi Marcela,

make sure you have this setting disabled:

pastedImage_1.png

I hope this helps,

Erich

在原帖中查看解决方案

2 回复数
3,123 次查看
BlackNight
NXP Employee
NXP Employee

Hi Marcela,

make sure you have this setting disabled:

pastedImage_1.png

I hope this helps,

Erich

3,122 次查看
marceladueñas
Contributor II

You are so brilliant!!, it solve all the errors and warnings.

Thank you so much.

Regards

0 项奖励
回复