Unknown macro: "existsRoute" (file: Drivers\Kinetis\SDHC_LDD.rgi)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unknown macro: "existsRoute" (file: Drivers\Kinetis\SDHC_LDD.rgi)

2,470件の閲覧回数
bowerymarc
Contributor V

I have a couple of projects (e.g. TWR-K60F120M_FatFS from mcuoneclipse) and when I load them I get three of these errors, line 103, 111, 96 of this file, which I can not find, and searching for the string "existsRoute" in the workspace yields nothing as well.  what's going on??

CWE 10.3...

ラベル(1)
タグ(1)
0 件の賞賛
返信
6 返答(返信)

2,310件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I just checked that project from GitHub, and I don't have that problem.

But the file name and error let me believe this is something inside the Processor Expert files, and somehow they are screwed up? Did you made an update or change to your installation recently?

Can you check what your about box says? I have

- CodeWarrior for MCU

     Version: 10.3

     Build Id:121211

I'm aware that there was an update on the web for a short period of time which has a problem: if you perform the update while you are debugging (or if you had a debug session right before the update), then this could have corrupted your installation.


Not sure if this is your problem.

0 件の賞賛
返信

2,310件の閲覧回数
bowerymarc
Contributor V

Mine is:

Installed Products:

- CodeWarrior for MCU

  Version: 10.3

  Build Id:121211

And the ProcessorExpert version:

  Processor Expert for MCU1.2.0.S_RT2_b1248-1334

How would (or... should?) I re-install processorExpert (guessing you're right about where the problem lies)?

0 件の賞賛
返信

2,310件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have the same version.

I believe your problem is in one of the files in

MCU\ProcessorExpert\Drivers

Drivers\Kinetis\SDHC_LDD.rgi is in one of the packages (not sure which one).

Are you sure you have not loaded any Processor Expert service packs for an addtional processor/CPU?

I ask because that error message let me believe something is missing.

0 件の賞賛
返信

2,310件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Here is what I have inside that folder:

3896_3896.png

Do you have the same?

0 件の賞賛
返信

2,310件の閲覧回数
bowerymarc
Contributor V

sorry just getting back to this... yes that file directory looks the same as mine, Eric.

here's the pe file....

0 件の賞賛
返信

2,310件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

closing the "Configuration Register" window should help to avoid the error. However could you please post here the ProcessorExpert.pe file from your project in order to reproduce it on our side?

best regards

Vojtech Filip

Processor Expert Support Team


0 件の賞賛
返信