USB_LDD Processor expert MK20DX256

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB_LDD Processor expert MK20DX256

1,284 次查看
carlosrc
Contributor I

Good morning

My name is Carlos. I'm working on the library USB_LDD for MK20dx256, a issue appear, it's necessary to set the clock input until 48Mhz. I tried it to configure the clock, but it's doesn't work. How can i configure the clock in a MK20DX256 to get 48Mhz?, I can't get it work.

Thanks,

Carlos

0 项奖励
回复
1 回复

1,110 次查看
adriancano
NXP Employee
NXP Employee

Hi,

You may find useful this posts on the MCU on Eclipse blog by Erich Styger:

USB MSD Host for the FRDM-K20D50M Board | MCU on Eclipse

USB CDC with the FRDM-K20D50M | MCU on Eclipse

Check the information there and say: Thank you Erich!.


Hope this information can help you,

Best Regards,

Adrian

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复