UART module 0 from kl25z128m4 is missing in KSDK + PE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UART module 0 from kl25z128m4 is missing in KSDK + PE?

Jump to solution
2,058 Views
matheuspinto
Contributor II

Hello,

When using KSDK + PE and choosing the fsl_uart component, the devices available are UART1 and UART2.

But, the UART0 does not appear! How I proceed?

Thanks

0 Kudos
Reply
1 Solution
1,754 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Matheus,

If you want to use the UART0 you need to use the fsl_lpsci component:

pastedImage_1.png

pastedImage_2.png

This is because the UART modules are supported by different HAL/drivers, the UART0 module is supported by the LPSCI HAL/driver and the UART1 and UART2 modules are supported by UART HAL/driver.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,755 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Matheus,

If you want to use the UART0 you need to use the fsl_lpsci component:

pastedImage_1.png

pastedImage_2.png

This is because the UART modules are supported by different HAL/drivers, the UART0 module is supported by the LPSCI HAL/driver and the UART1 and UART2 modules are supported by UART HAL/driver.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,754 Views
matheuspinto
Contributor II

Thanks Carlos,

It works! I felt a lack of documentation about the Kinetis sdk! Where would I found about this, if not on Kinetis forum?

Att,

Matheus

0 Kudos
Reply