TimeUnit_LDD clock source selection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TimeUnit_LDD clock source selection

跳至解决方案
1,938 次查看
henryxin
Contributor II

Hi there,

I have a question when I use the TimeUnit_LDD component in my KL25Z test project as:

(First I used LPTMR_CNR as a counter, I can choose different clock sources)

clk_LPTMR.png

it can be explained as datasheet:

datasheet_LPTMR.png

but when I try to use a TPM_CNT as a counter, there is no options in the Process Export Software for me to select the clock source as:clk_TPM1.png

but the datasheet says there are three clock source options as:

datasheet_TPM1.png

Is there anything I missed or misunderstand?

Thanks in advance.

Henry Xin

0 项奖励
回复
1 解答
1,735 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello henry xin:

The TPM clock source is configured as par of the system clocks in the CPU component:

pastedImage_0.png

Regards!

Jorge Gonzalez

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,736 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello henry xin:

The TPM clock source is configured as par of the system clocks in the CPU component:

pastedImage_0.png

Regards!

Jorge Gonzalez

0 项奖励
回复
1,735 次查看
henryxin
Contributor II

Hi Gonzalez,

Thanks.

I missed the TPM part in the CPU component.

Best Regards,

Henry Xin

0 项奖励
回复