TimeUnit_LDD clock source selection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TimeUnit_LDD clock source selection

ソリューションへジャンプ
2,012件の閲覧回数
henryxin
Contributor II

Hi there,

I have a question when I use the TimeUnit_LDD component in my KL25Z test project as:

(First I used LPTMR_CNR as a counter, I can choose different clock sources)

clk_LPTMR.png

it can be explained as datasheet:

datasheet_LPTMR.png

but when I try to use a TPM_CNT as a counter, there is no options in the Process Export Software for me to select the clock source as:clk_TPM1.png

but the datasheet says there are three clock source options as:

datasheet_TPM1.png

Is there anything I missed or misunderstand?

Thanks in advance.

Henry Xin

ラベル(2)
0 件の賞賛
返信
1 解決策
1,809件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello henry xin:

The TPM clock source is configured as par of the system clocks in the CPU component:

pastedImage_0.png

Regards!

Jorge Gonzalez

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,810件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello henry xin:

The TPM clock source is configured as par of the system clocks in the CPU component:

pastedImage_0.png

Regards!

Jorge Gonzalez

0 件の賞賛
返信
1,809件の閲覧回数
henryxin
Contributor II

Hi Gonzalez,

Thanks.

I missed the TPM part in the CPU component.

Best Regards,

Henry Xin

0 件の賞賛
返信