TSI with K20

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSI with K20

1,419 Views
night
Contributor II

Hello,

I'm trying to use TSI peripheral with kinetis k20 and processor expert. I'm working with CodeWarrior 10.2. When I select the TSI_LDD and add it to the project, Component Inspector say me "Target CPU does not contain peripheral of this types", but K20 has it, and the eval board too. Why? How can I use it?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,216 Views
vfilip
NXP Employee
NXP Employee

Hello,

TSI_LDD should not be used. I would recommend to install the newest version of CW V10.3 and create project with TSS_Libray component.

Tutorial: Touching the Freedom KL25Z Board | MCU on Eclipse

CodeWarrior: freescale.com/codewarrior

best regards

Vojtech Filip

Processor Expert Support Team


0 Kudos
Reply