Setting loopback request in PCIe training sequence via T2080 RC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting loopback request in PCIe training sequence via T2080 RC

1,281 次查看
scottgerhold
Contributor IV

I am trying to use Serdes Val to test a link that has a switch on the other end. The switch can be configured to go into a loopback mode if the T2080 were to set the loopback bit in the TS1 sequence. Can the tool be used to push the external EP into that mode? Is there anything in the T2080 register space that I can configure via SW or an emulator to set that bit in the training sequence?

0 项奖励
回复
0 回复数