Setting loopback request in PCIe training sequence via T2080 RC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting loopback request in PCIe training sequence via T2080 RC

1,290件の閲覧回数
scottgerhold
Contributor IV

I am trying to use Serdes Val to test a link that has a switch on the other end. The switch can be configured to go into a loopback mode if the T2080 were to set the loopback bit in the TS1 sequence. Can the tool be used to push the external EP into that mode? Is there anything in the T2080 register space that I can configure via SW or an emulator to set that bit in the training sequence?

0 件の賞賛
返信
0 返答(返信)