Selected processor does not support PinSettings component: "MKL26Z256MC4"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Selected processor does not support PinSettings component: "MKL26Z256MC4"

ソリューションへジャンプ
1,587件の閲覧回数
alexlesuper
Contributor I

Hello,

We are basing our next product on the Low-power L series processor with USB support. Specifically, the chip we are using is the MKL26Z256MC4. I am building the processor expert project and I want to use the Freescale PinSettings configuration to rename the pins and route them to the appropriate peripherals. However, when I try to instantiate the right component, it gives me an error message of which I have pasted a screenshoPinsettingsNotSupported.PNG.pngt.

To my knowledge, this is not a legacy part, so why is the PinSettings component not working?

Thanks,

Alex

0 件の賞賛
返信
1 解決策
1,497件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Alex,

I have find out that the MKL26Z256 derivatives support (Processor Expert with Kinetis SDK) is not published yet. These derivatives will be available in the Kinetis SDK 1.2.0 release (the release is planned at the end of April 2015).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,498件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Alex,

I have find out that the MKL26Z256 derivatives support (Processor Expert with Kinetis SDK) is not published yet. These derivatives will be available in the Kinetis SDK 1.2.0 release (the release is planned at the end of April 2015).

Best Regards,

Marek Neuzil

0 件の賞賛
返信