SSI_LDD clock bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,122件の閲覧回数
bowerymarc
Contributor V

Setting the "Master Clock" to "Input Pin" in SSI_LDD results in this code in Audio0_Init (default name):

  /* I2S0_MCR: MOE=0 */

  I2S0_MCR &= (uint32_t)~(uint32_t)(I2S_MCR_MOE_MASK); /* Disable MCLK divider */

  while ((I2S0_MCR & I2S_MCR_MOE_MASK) != 0U) {} /* Wait for MCLK disable*/

  /* I2S0_MDR: ??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,FRACT=0,DIVIDE=0xF9 */

  I2S0_MDR = (I2S_MDR_FRACT(0x00) | I2S_MDR_DIVIDE(0xF9)); /* Configure Mclk divide ratio */

  /* I2S0_MCR: DUF=0,MOE=1,??=0,??=0,??=0,??=0,MICS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  I2S0_MCR = (I2S_MCR_MOE_MASK | I2S_MCR_MICS(0x00)); /* Configure Mclk source */


Last line: MOE is set, making the MCLK line an output.


ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,944件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

thanks for reporting this bug to us. We will fix it for next release (I am not sure about CW V10.6 because we are close to this release. However this fix is going to be part of DriverSuite 10.4).

Best regards

Vojtech Filip

Processor Expert Support Team

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,945件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

thanks for reporting this bug to us. We will fix it for next release (I am not sure about CW V10.6 because we are close to this release. However this fix is going to be part of DriverSuite 10.4).

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信
1,944件の閲覧回数
bowerymarc
Contributor V

any workaround?

0 件の賞賛
返信
1,944件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

sorry I have omitted that. I think there are two possible ways how to workaround it. Either freeze generated code of this component by right click on component and use "Dont Write...." menu command or write the correct value into I2S0_MCR just after calling initialization method.

I2S0_MCR = I2S_MCR_MICS(0x00);       /* Configure Mclk source */

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信