SPI communication FRDM-KL46Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI communication FRDM-KL46Z

ソリューションへジャンプ
3,086件の閲覧回数
r58737
NXP Employee
NXP Employee

HEllo ,

I'm using a FRDM board to send SPI command to an external part with processor expert and  SM1: SPImaster_LDD component.

here below the component configuration :

SM1_SPImaster LDD.png

To send a SPI write command I used the following functions  and it's working fine:( I 'm using a GPIO to drive the CS)

static  uint8_t SpiWriteReg(uint8_t addr, uint8_t val) {

  SPI_CS_ENABLE();

  SPIWriteByte(addr); /* address */

  SPIWriteByte(val) ; /* data */

  SPI_CS_DISABLE();

  return ERR_OK;

}

static void SPIWriteByte(unsigned char write) {

  unsigned char dummy; 

  (void)SM1_ReceiveBlock(SM1_DeviceData, &dummy, sizeof(dummy));

  (void)SM1_SendBlock(SM1_DeviceData, &write, sizeof(write));

  while(!spi_DataReceivedFlag){}

}

But I have a problem with such commands, because there is a delay between both SPIWriteByte(adrr) & SPIWriteByte(val).

Could someone explain me how to send the same information without any delay as shown in the below picture:


SPI scope.png

Thanks for your help

Rgds

Philippe


タグ(3)
0 件の賞賛
返信
1 解決策
2,115件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Philippe,

It seems that your code contains sending of address and data in two block (SendBlock method). To minimize the delay you must use SendBlock method and send address and data in one block (the SPIMaster_LDD code is optimized for this usage). You can use a structure where the addr and val are defined e.g.

typedef struct {

  uint8_t addr;

  uint8_t val;

} tData;

Then the code of your SpiWriteReg function can be following:

static  uint8_t SpiWriteReg(uint8_t addr, uint8_t val) {

  tData data;

  // data preparation for sending in one block of data

  data.addr = addr;

data.val = val;

  // dummy variable for receiving of data

uint8_t dummy[2];

SPI_CS_ENABLE();

  // send and receive of address and value

(void)SM1_ReceiveBlock(SM1_DeviceData, &dummy, sizeof(tData));

(void)SM1_SendBlock(SM1_DeviceData, &data, sizeof(tData));

  // wait for receiving of the block of data

while(!SM1_GetBlockReceivedStatus(SM1_DeviceData)){}

  SPI_CS_DISABLE();

  return ERR_OK;

}

Please, note that you can also use GetBlockReceiveStatus method of the SPIMaster_LDD component. You will find it when you switch to Advanced view mode in to the Component Inspector and enable generation of this method.

For more information about SPIMaster_LDD see the help of this component accessible using pop-up menu of the component in the components view(description of methods and Typical Usage).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,116件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi Philippe,

It seems that your code contains sending of address and data in two block (SendBlock method). To minimize the delay you must use SendBlock method and send address and data in one block (the SPIMaster_LDD code is optimized for this usage). You can use a structure where the addr and val are defined e.g.

typedef struct {

  uint8_t addr;

  uint8_t val;

} tData;

Then the code of your SpiWriteReg function can be following:

static  uint8_t SpiWriteReg(uint8_t addr, uint8_t val) {

  tData data;

  // data preparation for sending in one block of data

  data.addr = addr;

data.val = val;

  // dummy variable for receiving of data

uint8_t dummy[2];

SPI_CS_ENABLE();

  // send and receive of address and value

(void)SM1_ReceiveBlock(SM1_DeviceData, &dummy, sizeof(tData));

(void)SM1_SendBlock(SM1_DeviceData, &data, sizeof(tData));

  // wait for receiving of the block of data

while(!SM1_GetBlockReceivedStatus(SM1_DeviceData)){}

  SPI_CS_DISABLE();

  return ERR_OK;

}

Please, note that you can also use GetBlockReceiveStatus method of the SPIMaster_LDD component. You will find it when you switch to Advanced view mode in to the Component Inspector and enable generation of this method.

For more information about SPIMaster_LDD see the help of this component accessible using pop-up menu of the component in the components view(description of methods and Typical Usage).

Best Regards,

Marek Neuzil

0 件の賞賛
返信
2,115件の閲覧回数
r58737
NXP Employee
NXP Employee


Hello Marek,

thanks for your help. that is what I was looking for.

Rgds

Philippe

0 件の賞賛
返信