SPI bus speed/frequency for Kinetis / K60F120

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPI bus speed/frequency for Kinetis / K60F120

跳至解决方案
2,883 次查看
PeterFromSweden
Contributor III

Hi

 

It is not possible to select maximum frequency for SPI bus in Procesor Expert.

 

K60P144M150SF3RM chapter 3.9.5.2 clearly states that it is internal bus clock / 2.

Processor Expert Driver Suite 10.0.0 doesn't offer this. Is it wrong in Kinetis manual or in Processor Expert?

See pictures below.

 

/Peter

3405_3405.jpgKinetis SPI clock.jpg3404_3404.jpgKinetis Clocks.jpg

Original Attachment has been moved to: ProcessorExpert.pe.zip

0 项奖励
回复
1 解答
2,028 次查看
vfilip
NXP Employee
NXP Employee

Hello,

this is PEx issue and it would be fixed in the next release (new version should be available within two weeks). The list of pre-calculated values is not complete, however as workaround it should be possible to enter 30 MHz directly into Init.value field.

best regards

Vojtech Filip

Processor Expert Support Team


在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,028 次查看
DavidS
NXP Employee
NXP Employee

Hi Peter,

To add to the responses, the RM quite often speaks of the capability of the silicon IP module and not what was implement or specified differently.

Rule of Thumb is Section #3 of RM has what is implemented in the device.

Ex:

   Section #3 might say there are 3 SPI moduled and each has 3 chip selects.

   Module Section might say the SPI module can have 100 chip select (I'm exagerating to make point)

Unfortunately Section #3 doesn't include pin limitation and you must consult the respective Data Sheet.

For the K60 120MHz device you are using the Section 6.8.7 DSPI switching specifications has Host max frequency of 30MHz and as Slave 15MHz.

Hope this helps.

Regards,

David

2,028 次查看
vfilip
NXP Employee
NXP Employee

Hello,

could you please post here the ProcessorExpert.pe file from your project in order to analyze your issue?

best regards

Vojtech Filip

Processor Expert Support Team

0 项奖励
回复
2,028 次查看
PeterFromSweden
Contributor III

Hi

I updated the original question with requested attachment.

Regards

/Peter

0 项奖励
回复
2,029 次查看
vfilip
NXP Employee
NXP Employee

Hello,

this is PEx issue and it would be fixed in the next release (new version should be available within two weeks). The list of pre-calculated values is not complete, however as workaround it should be possible to enter 30 MHz directly into Init.value field.

best regards

Vojtech Filip

Processor Expert Support Team


0 项奖励
回复