SBC uja1169 CMC configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SBC uja1169 CMC configuration

ソリューションへジャンプ
3,244件の閲覧回数
fk1
Contributor I

Hi,

I'm using the SBC UJA1169 middleware component

after being unable to perform CAN communications, i noticed that the processor expert output sets the CMC inside the CAN control register to SBC_UJA_CAN_CMC_OFMODE,
f i manually change the CMC in the config to SBC_UJA_CAN_CMC_ACMODE_DD, i can get the processor to receive CAN data.

how do i get processor expert to automatically set the CMC to another value, i can not see anything in the configuration what looks like it would change this?

 

note: I'm using S32 DS 2.0 on the processor S32K144

fk1_0-1626868870561.png

fk1_1-1626869161137.png

 

 

0 件の賞賛
返信
1 解決策
3,230件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

checking the same in my S32DS2.2 with SDK RTM 3.0.3 I see option for mode selection

PetrS_0-1626942081487.png

So I can recommend to update S32DS and SDK; refer to https://community.nxp.com/t5/S32-Design-Studio/bd-p/s32ds

BR, Petr

元の投稿で解決策を見る

2 返答(返信)
3,231件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

checking the same in my S32DS2.2 with SDK RTM 3.0.3 I see option for mode selection

PetrS_0-1626942081487.png

So I can recommend to update S32DS and SDK; refer to https://community.nxp.com/t5/S32-Design-Studio/bd-p/s32ds

BR, Petr

3,217件の閲覧回数
fk1
Contributor I

Hi Petr,

 

I downloaded S32 DS 3.4, and that setting is also available

fk1_0-1627304953454.png

 

 

Thanks

Fahed

0 件の賞賛
返信