S32K148 QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 QSPI

2,387件の閲覧回数
trunghieudon
Contributor I

I ran the S32K148 QSPI example given within the s32ds and It was stuck inside the error trap loop. I saw many thread having the same problem. Did anyone figure out why there was such an error?

This is the one that I used: 

https://www.nxp.com/docs/en/application-note/AN12193.pdf 

AN12193SW:

https://www.nxp.com/webapp/Download?colCode=AN12193SW&docLang=en 

タグ(3)
0 件の賞賛
返信
1 返信

2,332件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello Austin,

In the SDK there's an example that uses the same peripheral, in the getting started for this example specify the following modifications that need to be done to run it:

pastedImage_1.png

Did you do these modifications?

Best Regards,

Alexis Andalon

0 件の賞賛
返信