S32K144 processor with Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 processor with Processor Expert

2,664 Views
gerardiborra
Contributor I

Hello,

I'm trying to add to my project a Processor Expert file but I have this issue

pastedImage_2.png

pastedImage_1.png

What is the problem?

Thanks.

0 Kudos
Reply
2 Replies

1,787 Views
raresvasile
NXP Employee
NXP Employee

Hi,

1. Can you provide the steps that you took to add the ProcessorExpert support to the project? We need them in order to reproduce the issue as closely as we can.

2. Please replace C:\NXP\KSDK_1.3.0 in Project Properties->ProcessorExpert->S32 SDK specific with ${ProcessorExpert_loc}/../../S32DS/S32_SDK_EAR_0.8.2. This may resolve the issue as the SDK path should be pointing to a valid S32 SDK location.

Thank you,

Rares

0 Kudos
Reply

1,787 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I am not sure what you mean by the " add to my project a Processor Expert file" but the error that is reported mean that the Processor Expert project has been created by using KSDK 1.1 but the selected path refers the KSDK 1.3.0 version. I.e. the version of the KSDK is not the same and conversion of the components (from the version 1.1 to 1.3.0)  may impact settings and functionality of the Processor Expert components (new version of the KSDK drivers).

Best Regards,

Marek Neuzil

0 Kudos
Reply