S12ZVL64 cant receive data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL64 cant receive data

1,307 Views
yongd丁
Contributor I
the code reference to "ZVC192-IIC-HUMIDITY-CW106"(master mode/Non-interrupt mode )
//**********************************************************************************************
void Init_IIC(void);
void IIC_Start(void);
void IIC_Stop(void);
void IIC_RepeatStart(void);
void IIC_Delay(void);
void IIC_CycleWrite(byte bout);
byte IIC_CycleRead(byte ack);
void IIC_SendBlock(uint8_t address,uint8_t *WrPointer,uint8_t WrNumber,uint8_t mode);
void IIC_RecvBlock(uint8_t address,uint8_t *rdpointer,uint8_t rdNumber);
//**********************************************************************************************
// Private memory declarations
//**********************************************************************************************
static byte error;
static word timeout;
//==============================================================================
// Init_IIC module
//==============================================================================
void Init_IIC(void)
{
 IIC0IBFD = 0x80;   //Frequency divider register
     //see attached IIC calculator in excel file
 IIC0IBAD = 0x00;   //Slave address of this module;
 IIC0IBCR = 0x80;   //Enable I2C module, No interrupts;
}
//*********************************************************
// Initiate IIC Start Condition
//*********************************************************
void IIC_Start(void)
{
  IIC0IBCR_MS_SL = 1;
  timeout = 0;
  while ((!IIC0IBSR_IBB) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error |= 0x01;
} //*** Wait until BUSY=1

//*********************************************************
// Initiate IIC Stop Condition
//*********************************************************
void IIC_Stop(void)
{
  IIC0IBCR_MS_SL = 0;
  timeout = 0;
  while ( (IIC0IBSR_IBB) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error |= 0x02;
} //*** Wait until BUSY=0

//*********************************************************
// Initiate IIC Repeat Start Condition
//*********************************************************
void IIC_RepeatStart(void)
{
  IIC0IBCR_RSTA = 1;
  timeout = 0;
  while ((!IIC0IBSR_IBB) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error |= 0x04;
} //*** Wait until BUSY=1

//*********************************************************
// IIC Delay
//*********************************************************
void IIC_Delay(void)
{
  byte IICd;
  for (IICd=0; IICd<100; IICd++){};
}

//*********************************************************
// IIC Cycle Write
//*********************************************************
void IIC_CycleWrite(byte bout)
{
  timeout = 0;
  while ((!IIC0IBSR_TCF) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error |= 0x08;
  IIC0IBDR = bout;
  timeout = 0;
  while ((!IIC0IBSR_IBIF) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error |= 0x10;
  IIC0IBSR_IBIF = 1;
  if (IIC0IBSR_RXAK)
    error |= 0x20;
}

//*********************************************************
// IIC Cycle Read
//*********************************************************
byte IIC_CycleRead(byte ack)
{
  byte bread;
  timeout = 0;
  while ((!IIC0IBSR_TCF) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error|=0x08;
  IIC0IBCR_TX_RX = 0;
  IIC0IBCR_TXAK = ack;
  bread = IIC0IBDR;
  timeout = 0;
  while ((!IIC0IBSR_IBIF) && (timeout<1000))
    timeout++;
  if (timeout >= 1000)
    error |= 0x10;
  IIC0IBSR_IBIF=1;
  return bread;
}
///////////////////////////////////////////////////////////////////////
void IIC_SendBlock(uint8_t address,uint8_t *WrPointer,uint8_t WrNumber,uint8_t mode)
{
 uint8_t i;
 IIC0IBCR_TX_RX = 1;
 IIC_Start();
 IIC_CycleWrite(address&0xfe);
 for(i=0;i<WrNumber;i++)
 {
  IIC_CycleWrite(*WrPointer);
  WrPointer++; 
 }
 if(mode==0)IIC_Stop();
}
///////////////////////////////////////////////////////////////////////////////////
void IIC_RecvBlock(uint8_t address,uint8_t *rdpointer,uint8_t rdNumber)
{
 uint8_t i;
 uint8_t send_ack=0;
 IIC0IBCR_TX_RX = 1;
 IIC_RepeatStart();
 IIC_CycleWrite(address|0x01);
 for(i=0;i<rdNumber;i++)
 { 
  if(i==(rdNumber-1))send_ack=1;
  else send_ack=0;
  *rdpointer=IIC_CycleRead(send_ack);
  rdpointer++;
 }
 IIC_Stop();
}
0 Kudos
Reply
0 Replies