Restart status register RCM SRS1 Jtag bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Restart status register RCM SRS1 Jtag bit

1,319件の閲覧回数
viktorkarlsson
Contributor I

Hi 
I have problem with random restarts is trying to figure out the reason.
I'm using a K66 Kinnetis with a jlink segger base debugger using jtag chain.

I run in debug mode and catch restart in the reset interrupt handler.

The RCM SRS1 jtag bit i set and documentation say:

Indicates a reset has been caused by JTAG selection of certain IR codes: EZPORT, EXTEST, HIGHZ,
and CLAMP.

Is there more info to get or is that it?

0 件の賞賛
返信
1 返信

1,212件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

 

 

Hello

 

This issue may be caused by hardware. I suggest you make sure that the external pull up/down resistors are connected to the circuit.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

0 件の賞賛
返信