RT595 DSP file stopped, unsupported format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT595 DSP file stopped, unsupported format

4,250件の閲覧回数
eagan_yu
Contributor III

HI

   I would really appreciate it if you could give me some advice and help !
   Recently I was using the RT595 development board and when I was using the SDK routines, I had a problem that the DSP was unable to decode my MP3 audio files.
And I use the SDK example is : evkmimxrt595_dsp_xaf_demo_cm33
And the Log is Follows:

>> file list
Available audio files:
Happy.mp3
Wild.mp3
Stay.mp3
>> file Stay.mp3
DSP file stopped, unsupported format.
[APP_DSP_IPC_Task] response from DSP, cmd: 12, error: 1
DSP file playback start failed! return error = 1
>> file Wild.mp3
[APP_DSP_IPC_Task] response from DSP, cmd: 12, error: 0
DSP file playback start
>> DSP file playback complete


Above, you can see, different music files, some can not decode successfully, I want to know why, by the way, my music files downloaded from QQ music app.

B&R
Eagan

0 件の賞賛
返信
6 返答(返信)

4,041件の閲覧回数
eagan_yu
Contributor III

Hi @jingpan 

There seems to be a problem with the bit rate of the music file,

I tried to convert the bit rate of the MP3 file, and suddenly the song can play.

Regards,

Eagan

 

 

0 件の賞賛
返信

4,044件の閲覧回数
eagan_yu
Contributor III

Hi @jingpan 

Follow your advice. I tried, but it didn't solve the problem.

Regards,

Eagan

0 件の賞賛
返信

4,203件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

HI @eagan_yu ,

The DSP can't recognize/play the file due to metadata (song name, alburm, art, etc) at the front of the mp3 frame data. You can use M33 to parse the MP3 file and filter the data.

 

Regards,

Jing

0 件の賞賛
返信

4,152件の閲覧回数
eagan_yu
Contributor III

Hi Jing

Thank for you reply.

I want to Know , do you mean to filter out the  ID3V2 data ?

The MP3 file is divided into three parts: TAG_V2(ID3V2), Frame, and TAG_V1(ID3V1).

0 件の賞賛
返信

4,148件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Yes, I think so.

 

Regards,

Jing

0 件の賞賛
返信

4,227件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @eagan_yu ,

I'll check with software team. Please wait.

 

Regards,

Jing

0 件の賞賛
返信