ProcessorExpert.pe disabled? How?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ProcessorExpert.pe disabled? How?

4,174件の閲覧回数
F50SC
Contributor III

Hi

I've been working on a project for a while with KDS 3.0 & KSDK 1.20.....and now ProcessorExpert does not allow me to generate code???

pastedImage_0.png

I don't know what I've done to cause this error....but cannot find anything under project properties to re-enable?

I also see this in the Component Inspector for the selected MCU....

pastedImage_1.png

These are the settings for PE under Project Properties>ProcessorExpert

pastedImage_2.png

and Project Properties>Processor Expert>Kinetis SDK Specific

pastedImage_4.png

The MCU I'm using is MK24FN1M0VLL12 in 100pin LQFP pack....I don't know why it is showing Selected processor does not support SDK, as the project was created as SDK & PE project based

on MCU and have been generating code from PE, compiling & debugging on the target without issues till now.

Does anyone know how to renable PE?

タグ(2)
0 件の賞賛
返信
7 返答(返信)

3,844件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Jerome,

in your project, Processor Expert is disabled, see Project > Properties > Disable Processor Expert changes (actually it is shown in one of your screenshots). Change the value from "Yes" to "No", this will enable the code generation:

ProcessorExpertDisabled.PNG

Regards,

Lukas

0 件の賞賛
返信

3,844件の閲覧回数
F50SC
Contributor III

Hi Lukas

Thanks for that....I'm a bit embarrassed I didn't see the option myself....even in the screenshots. At least I wasn't the only one :smileysilly:

The question I still have is how it got disabled in the first place? I didn't even know of the option yet I have been generating code from PE for sometime without it ever being disabled.

KDS+PE does some strange things at times.

Thank again.

Regards

Jerome

0 件の賞賛
返信

3,844件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pitt,

please screenshot the view as this :

pastedImage_0.png

And please send your project to me , i will test it on my side .

And have you install the KSDK1.2 successfully ?

BR

Alice

0 件の賞賛
返信

3,844件の閲覧回数
F50SC
Contributor III

Hi Alice

Yes, KSDK 1.2.0 is installed successfully, something broke with the project and caused PE to be disabled.

0 件の賞賛
返信

3,844件の閲覧回数
F50SC
Contributor III

Update.....

I created a new project as before, same MCU, standalone project NOT linked.

Added my source files to the sources folder.

Imported "Apply Board Configuration.pbe" into ProcessorExport.pe from my project that I exported beforehand.

No I'm backup and generating code....PE is enabled!

0 件の賞賛
返信

3,844件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Yes , when you create project ,please select "Standalone" :

pastedImage_0.png

Hope it helps

Alice

0 件の賞賛
返信

3,844件の閲覧回数
F50SC
Contributor III

Hi Alice

I meant to say..."Now I'm backup and generating code....PE is enabled!"

This was after I opened a new project, copied my source files over AND imported my PE settings.

Standalone project was selected when I created a new project.

0 件の賞賛
返信