Processor expert code generation script error with DAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor expert code generation script error with DAC

1,813 Views
il_mix
Contributor II

Hi,

I am trying to use the DAC using the micro controller MCF51MM256CLK with code warrior.

I've added the Init_DAC component from Peripheral Initialization.

Generating the processor expert code I obtained this error:

ERROR: Unexpected status of the scripts: Drivers\HCS08\Init_DAC_HCS08.rgi

I also noticed that in the list of supported item the MCF51MM256CLK is not listed, while I can find MCF51MM256_80/81/100/104. I don't know if the MCF51MM256CLK can be use anyway.

Could someone help me to fix this problem?

Thank you in advance!

0 Kudos
Reply
1 Reply

1,582 Views
cristianzamfire
NXP Employee
NXP Employee

    Hello,

    I could not reproduce the issue, I tried the Init_DAC component on the MCF51MM256CLK  CPU with various settings and I never had any generation error. I used CodeWarrior 10.6.

    Regarding the CPU, you can select the MCF51MM256CLK variant by adding a new CPU from the Component Library, Processors tab. A list with all available variants will be displayed. MCF51MM256CLK is the 80-pin variant.

    Best Regards,

    Cristian

0 Kudos
Reply