Processor Expert

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert

Jump to solution
4,600 Views
Klayton
Contributor III

Running CW 10.1 with latest updates.  When I use the new project wizard to create a new project for a K10 processor the processor expert sits at 50% then times out.  Here is the message from the console:

 

System directory = C:\Program Files\Freescale\CW MCU v10.1\MCU\ProcessorExpert
User working directory = C:\Documents and Settings\All Users\Application Data\Processor Expert\CWMCU_PE5_00
2011-10-28 13:01:01 Connecting to Processor Expert service at localhost:9999 ...
2011-10-28 13:01:02 Starting local service ...
2011-10-28 13:01:22 Connecting to Processor Expert service at localhost:9999 ...
2011-10-28 13:01:22 Sucessfully connected to Processor Expert service, waiting for start-up.
2011-10-28 13:01:24 Processor Expert successfully started:
product version: 5.2, product info: for Freescale Microcontrollers, core version: 04.49.
Timeout for creating PE/DI project. Canceling the Job.

 

Anyone have any suggestions?

Thanks

0 Kudos
Reply
1 Solution
4,117 Views
ProcessorExpert
Senior Contributor III

Hello,

 

PEx one-time needs to update its databases after installing each SP (updating of cdb files) and in case you start creation of new project during this action it could lead to the behavior as is described.

To avoid the problem please follow one of the steps below (A or B):  

 

Option A:
Restart your CW and wait till all progress bar stop running. After that please continue with creation of a new project.

Option B:
1 - Close CW
2 - Run PEsrv.exe manually from the following folder: {CodeWarrior}/MCU/ProcessorExpert/
3 - Wait till it will not allocate any CPU resources
4 - Start CW

 

This behaviour should be imrpoved in CW V10.2.

 

best regards
Vojtech Filip
Processor Expert Support Team

View solution in original post

0 Kudos
Reply
5 Replies
4,117 Views
ProcessorExpert
Senior Contributor III

Hello,

 

PEx one-time needs to update its databases after installing each SP (updating of cdb files) and in case you start creation of new project during this action it could lead to the behavior as is described.

To avoid the problem please follow one of the steps below (A or B):  

 

Option A:
Restart your CW and wait till all progress bar stop running. After that please continue with creation of a new project.

Option B:
1 - Close CW
2 - Run PEsrv.exe manually from the following folder: {CodeWarrior}/MCU/ProcessorExpert/
3 - Wait till it will not allocate any CPU resources
4 - Start CW

 

This behaviour should be imrpoved in CW V10.2.

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply
4,117 Views
Klayton
Contributor III

Vojtech,

Tried both options and got the same error as before.  Any other ideas?

 

Thanks,

Klayton

0 Kudos
Reply
4,117 Views
ProcessorExpert
Senior Contributor III

Could you please give us more details on your configuration to allow reproducing the problem?

- What operating system are you using ? (windows version, 32 or 64 bit, language etc.)

- What servicepacks have you applied to the CodeWarrior ?

- Have you installed the CW and servicepakcs with administrator rights ?

 

 

best regards
Petr Hradsky
Processor Expert Support Team


0 Kudos
Reply
4,117 Views
Klayton
Contributor III

System is windows XP 32 bit.

 

I have used the install new software dialog in the help menu in code warrior to install all available stuff.

 

Here is what the help screen says my build ID etc.. is:

 

CodeWarrior Development Studio

Version: 1.0.0
Build Id: b15_2105-A22

(c) Freescale Semiconductor, Inc. 2010. All rights reserved.
Learn more about CodeWarrior at
http://www.freescale.com/codewarrior

Installed Products:
- CodeWarrior for MCU
Version: 10.1
Build Id:110204

 

 

Here is what the install software dialog box (from help menu) says I have installed:

 

CodeWarrior ARM Debugger 10.1.1.FSL_b0982
CodeWarrior ARM Debugger 10.1.1.FSL_b0982
CodeWarrior ColdFire Debugger 10.1.1.FSL_b5481
CodeWarrior Core Debugger 7.15.1.FSL_b8726
CodeWarrior Core Debugger NLS 7.15.1.FSL_b8726
CodeWarrior Core IDE 1.0.1
CodeWarrior HC(S)08 Debugger 10.1.1.FSL_b5491
CodeWarrior Kernel Awareness SDK 7.15.0.FSL_b8910
CodeWarrior Power Archtecture Debugger 10.0.1.FSL_b2241
CodeWarrior RS08 Debugger 10.1.1.FSL_b5491
CodeWarrior RS08 Debugger 10.1.1.FSL_b5491
ColdFire Database 1.0.2
CW MCU v10.1 Update 1.0.1
Kinetis Runtime 1.0.4
MCU 10.1.13
MCU Debug Connections 10.1.2.FSL_b5492
MCU v10.1 Compiler Update (ColdFire, Kinetis, Qorivva) 1.0.2
MCU v10.1 Service Pack for Kinetis 120MHz K10 K20 K70 K60 1.0.2
MCU v10.1 Service Pack for MC13233C 1.0.3
MCU v10.1 Service Pack for MC13234C/MC13238C 1.0.1
MCU v10.1 Service Pack for MC9S08PT60 1.0.3
MCU v10.1 Service Pack for MCF51JF128 1.0.3
MCU v10.1 Service Pack for MMA9550 1.0.4
MCU v10.1 Service Pack for PXD10xx/MPC560xS 1.0.1
MCU v10.1 Service Pack for PXD2020/MPC5645S 1.0.0
MCU v10.1 Service Pack for PXR4030/PXR4040/MPC5673F/MPC5674F 1.0.1
MCU v10.1 Service Pack for PXS20xx/MPC5643L 1.0.1
MCU v10.1 Service Pack for PXS30xx/MPC567xK 1.0.1
PPC Runtime for E200z0h Processor 1.0.0
Processor Expert Feature 1.0.7.b1131-0312
Processor Expert for 9S08PT60 1.0.0

 

As of today Code Warrior is still timing out before it creates the processor expert project.

 

Hope this helps.

 

Klayton

0 Kudos
Reply
4,117 Views
ProcessorExpert
Senior Contributor III

I'm sorry, but I haven't reproduced the problem. Maybe there is somehing corrupted in your installation.

I recommend trying to install a clean installation to different location:

 

#1 – Installation of CW V10.1

#2 – Installation of PE update 1.0.1 for CW V10.1 (installation process must end with restart of CW)

 

best regards
Petr Hradsky
Processor Expert Support and Servicepacks Team


0 Kudos
Reply