Processor Expert with IAR Compiler for Kinetis?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert with IAR Compiler for Kinetis?

ソリューションへジャンプ
3,152件の閲覧回数
RUssery
Contributor I

Greetings,

 

I'm having some trouble getting up and running with Processor Expert. I want to create some PWM drivers using PE for the IAR Embedded Workbench for ARM (EWARM) compiler for the Kinetis microcontroller.

 

Following are the specific things I need help with:

1) Are there any good "Getting Started" guides focusing on using Processor Expert with IAR EWARM?

2) Is there a standalone version of Processor Expert that supports IAR? I see such a version referenced in this document, but have not been able to locate a download for it.

3) If there is not a standalone version, how do I select the IAR compiler as the desired compiler while using PE under Codewarrior? I have CW 10.1 installed, and tried to run through the PE Getting Started Guide (PEXDRVGETSTARTEDUG), but when I got to the screen shown in Figure 5, IAR ARM C Compiler was not an option on the Target Compiler selection. Is there any way to enable this compiler option?

 

Thanks in advance!

 

Regards,

-Robert

0 件の賞賛
返信
1 解決策
2,568件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

This is the tool you need:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE

 

DOWNLOADS Tab:

 

http://cache.freescale.com/lgfiles/devsuites/HC08/ProcessorExpertDriverSuite5_2.Eclipse3_6.zip?fpsp=... - Debug, Compile and Build Tools&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=zip&WT_ASSET=Downloads&sr=1

 

 

 

Best Regards,

 

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,569件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

This is the tool you need:

 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE

 

DOWNLOADS Tab:

 

http://cache.freescale.com/lgfiles/devsuites/HC08/ProcessorExpertDriverSuite5_2.Eclipse3_6.zip?fpsp=... - Debug, Compile and Build Tools&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=zip&WT_ASSET=Downloads&sr=1

 

 

 

Best Regards,

 

Luis

0 件の賞賛
返信
2,568件の閲覧回数
RUssery
Contributor I

Thanks for the help and quick response! I guess I was confused by the fact that PE requires Eclipse to host it... I have it working now, and think I'm on the road to success. Thanks!

 

Regards,

Robert

0 件の賞賛
返信
2,568件の閲覧回数
microeval
Contributor I

Hi Robert,

I am facing same issue, not able to get the IAR ARM C compiler option in the code warrior IDE.

any suggestions?

I have code warrior 10.5 version.

Thanks in advance,

--Ram.

0 件の賞賛
返信