Processor Expert not working.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert not working.

3,583件の閲覧回数
rafaelzambrano
Contributor II

I am trying to add a component (BITIO) to my project. I get the following error "This component is not supported in Kinetis SDK project mode"

What d I need to set up in the tools or import so I can use those components?

Thank you.

Rafael-

0 件の賞賛
返信
6 返答(返信)

2,898件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It looks like you have created a project with the Kinetis SDK option. In that case, you cannot use any of the LDD (Logical Device Driver) components, only the fsl_* components will work, except you are using some of the McuOnEclipse components (which work both for SDK and non-SDK projects).

Erich

0 件の賞賛
返信

2,898件の閲覧回数
rafaelzambrano
Contributor II

Erich, Thank you for your answer. What would be the correct procedure to create the project and be able to use the LDD components. When I try to use the fsl components the system seems to accept them but I cannot get then to work properly. ie, I always get an error after I built the code. " function has not enough arguments" I thought with processor expert once you configured the component, you do not need to do anything else in the code when you are using the method. I am just trying to do a simple LED on and OFF and read the input value of a GPIO.

I looked at examples in Youtube but none of them use the fsl components. Any idea where can I go and look for some help in this matter.

0 件の賞賛
返信

2,898件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Rafael,

Please install the SDK to  your IDE .

For example , if use KDS,  please refer to here :

Writing your first toggle LED application with FRMD-K64F + KDS 1.1.0 + KSDK 1.0.0 Non-Processor Expe...

(install sdk to kds )

Tutorial: FreeRTOS with the Kinetis SDK and Processor Expert | MCU on Eclipse   (create PE project on sdk)

You can also refer to the "Getting Stared with Kinetis SDK.pdf"

BR

Alice

0 件の賞賛
返信

2,898件の閲覧回数
rafaelzambrano
Contributor II

Hello Alice,

I am using the TWR-K24F120M Evaluation board. The uC in the Board is MK24FN256VDC12 (121 MBGA).

0 件の賞賛
返信

2,898件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Rafael,

Yes , use the KSDK PE , the method TWR-K24 is the same with FRDM-K64 ().

Alice

0 件の賞賛
返信

2,898件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi, Rafael.

Please tell me which chip do you use ? and the SDK version ?


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信