Processor Expert is generating a .lcf file that is failing. How do I fix it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert is generating a .lcf file that is failing. How do I fix it?

1,739 Views
Symbolic
Contributor III

I am generating a "Bareboard" project using Processor Expert.

(This will be  a bootloader program, and this is why it is bareboard)

I have configured the system, and am generating the project (as is - no user code yet) using the FLASH configuration.

I am getting the linker warning:

>Segment m_data have to begin at address aligned to 512

>Please align ORIGIN of m_data segment to 512

The relevant part of the .lcf file is:

KEEP_SECTION { .vectortable }

KEEP_SECTION { .cfmconfig }

MEMORY {

  m_interrupts (RX) : ORIGIN = 0x1FFF0000, LENGTH = 0x000001E0

  m_text      (RX) : ORIGIN = 0x20000000, LENGTH = 0x00010000

  m_data      (RW) : ORIGIN = 0x1FFF01E0, LENGTH = 0x0000FE20

  m_cfmprotrom  (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010

}

Can I just ignore this warning?  (I don't expect so)

If not, how can I correct this situation?

I cannot just modify the .lcf file, as it is generated - as seen in the header section..

Using CW 10.5

Tags (2)
0 Kudos
Reply
2 Replies

1,475 Views
Symbolic
Contributor III

I am seeing this issue when generating the project for the RAM configuration also, it is not limited to the FLASH configuration.

0 Kudos
Reply

1,475 Views
BlackNight
NXP Employee
NXP Employee

You can fix the linker file by hand and disable the linker file generation. See point 8 in USB or not: CDC with Processor Expert | MCU on Eclipse